IMX93 ethosu_apps_rpmsg例程使用咨询

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX93 ethosu_apps_rpmsg例程使用咨询

1,443件の閲覧回数
chenyuansen
Contributor III

现在需要在imx93的m33核通过lpspi3驱动一块lcd屏幕,在ethosu_app_rpmsg中添加了spi相关的驱动后,可以通过编译,但是在执行时会触发段错误,代码在加载时没有运行到相关的信息打印阶段就触发了错误。同时我们基于ethosu_app_rpmsg例程移植测试uboot阶段加载m33固件,出现报错,log如附件log1所示,基于ethosu_app_rpmsg例程移植测试在内核阶段加载m33固件,同样出现报错,不过错误log不一样,log信息如附件log2所示,SDK版本是6.1.55,基于官方imx93 evk开发板测试,ethosu_apps_rpmsg例程是做什么的,看没有相关的readme.md,是不是有什么前置条件?

0 件の賞賛
返信
3 返答(返信)

1,419件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @chenyuansen 

 

I hope you are doing very well.

The Ethos-U65 NPU is integrated with NXP i.MX 93 processor and works in concert with the Cortex-M core and on-chip SRAM of the SoC.

Manuel_Salas_0-1745862745618.pngManuel_Salas_1-1745862768752.png

 

You can find all of these information in the i.MX Machine Learning User's Guide chapter 6.2.

 

There is explained how Ethos-U works.

 

Best regards,

Salas.

0 件の賞賛
返信

1,396件の閲覧回数
chenyuansen
Contributor III

目前就是按照第6.2章节这么用的,也是有同样的问题,将相关情况整理了一下,如附件所示

0 件の賞賛
返信

1,307件の閲覧回数
chenyuansen
Contributor III

Hi  Manuel,

这个问题是否可以帮忙继续分析一下呢

0 件の賞賛
返信