IMX93 FRDM board dts files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX93 FRDM board dts files

Jump to solution
46,485 Views
Et_MM
Contributor III

Hi,

I am working with the i.MX93 FRDM board. To build and run on this board, I cloned the following repository:
             git clone https://github.com/nxp-imx-support/meta-imx-frdm.git
 
However, after cloning, I couldn't find the corresponding DTS files for this board. Instead, I found many patch files.

Can you please help me with the procedure to obtain the DTS files for the i.MX93 FRDM board?
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
45,499 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Et_MM!

 

Apparently you have configured the machine to imx93-evk

Try following the steps that we provide in our github.

 

#Install the repo utility:
$: mkdir ~/bin
$: curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$: chmod a+x ~/bin/repo
$: PATH=${PATH}:~/bin

#Download i.MX Linux Yocto Release:
$: mkdir ${MY_YOCTO} # this directory will be the top directory of the Yocto source code
$: cd ${MY_YOCTO}
$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml
$: repo sync

If errors on repo init, remove the .repo directory and try repo init again.

#Integrate meta-imx-frdm recipes into the Yocto code base:
$: cd ./sources
$: git clone https://github.com/nxp-imx-support/meta-imx-frdm.git
$: cd meta-imx-frdm
$: git checkout imx-frdm-2.0

 

Change to the top directory of the Yocto source code and execute the command below to setup environment for build.

 

#For i.MX93 FRDM
$: MACHINE=imx93frdm DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-setup.sh -b frdm-imx93

 

Run the command below to generate Yocto images:

$: bitbake <image recipe>
 

Some image recipes:

Image Name Description
imx-image-core core image with basic graphics and no multimedia
imx-image-multimedia image with multimedia and graphics
imx-image-full image with multimedia and machine learning and Qt

 

Best Regards!

Chavira

View solution in original post

0 Kudos
Reply
18 Replies
46,471 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Et_MM!

Thank you for contacting NXP Support!

 

You can follow the steps that we provide in this community post.

 

If you have more inquiries please let me know.

 

Best Regards!

Chavira

0 Kudos
Reply
46,421 Views
Et_MM
Contributor III

Hi,

Thank you for the reply. 

I have tried the procedure mentioned in the community but bitbake is giving error. i have tried to rectify it but couldn't. Please go through the attachments shared and suggest me how to clear and go forward.

0 Kudos
Reply
46,410 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Et_MM!

 

I just compiled the SDK by my side without errors.

Maybe the error is due to you are using Ubuntu 24.

We recommend to use Ubuntu 22 for this job.

 

Best Regards!

Chavira

0 Kudos
Reply
46,379 Views
Et_MM
Contributor III

Hi,

Thank you for your reply. I tried this on Ubuntu 20, but during the BitBake execution, the process gets stuck at a certain point, and even my laptop freezes. I have tried multiple times, but it always freezes at the same point (as shown in the image I shared).

Is there a minimum system requirement for this process?

0 Kudos
Reply
46,368 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Et_MM!

Do you have the proper packages to compile?

 

Essential Yocto Project host packages are:

$ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential
chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils
iputils-ping python3-git python3-jinja2 python3-subunit zstd liblz4-tool file
locales libacl1

 

Try reducing the cores of the Yocto compilation adding the next lines in local.conf file:

BB_NUMBER_THREADS = "4"
PARALLEL_MAKE = "-j 4"

 

We recommend 4GB of ram of each core.

 

Best Regards!

Chavira

0 Kudos
Reply
46,353 Views
Et_MM
Contributor III

Hi,

From beginning itself i have installed the yocto hostage, its already mentioned in the community. In local.conf file i have added the 2 lines and tried but still it is freezing at the same point.
even i tried by adding

BB_NUMBER_THREADS = "2"
PARALLEL_MAKE = "-j 2"

still freezing but at different point comparing to previous. please check the shared image.

0 Kudos
Reply
46,312 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Et_MM!

Thank you for contacting NXP Support!

 

Those packages take too long time to compile, in my VM (16 cores and 64GB of RAM) takes over an a 90 minutes, the full compilation takes up to 5 or 6 hours, the full compilation of sdk can take a entire day to compile if your computer does not have the enough resources.

 

 

 

0 Kudos
Reply
46,289 Views
Et_MM
Contributor III

Hi

I understood what you are telling, but if the stuck issue is resolved then only the bitbake process will be completed. I want solution for this freezing, for that what to do?

Please go through the shared images and clarify whether it is ok for this bitbake process.

Is it because my system doesn't have enough resources it is freezing during bitbake? Is yes please share me what are the needed resources for this.

Again i tried bitbake today and it freezed but after doing some process,i have shared that image too.

 

0 Kudos
Reply
46,277 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Et_MM!

 

I understand the problem that you have but I can't do nothing by my side  since the problem is your host computer.

 

Try using another host computer or try using only one thread and one core to compile.

 

Best Regards!

Chavira

0 Kudos
Reply
45,653 Views
Et_MM
Contributor III

Hi,

I have done the bitbake process on ubuntu v22.4 and it is completed, as per the procedure mentioned in community till sdk installing i have done.

jesna@jesna-Latitude-5420:~/Yocto_SDK/bld-xwayland/tmp/deploy/sdk$ bash ./fsl-imx-xwayland-glibc-x86_64-imx-image-full-armv8a-imx93evk-toolchain-6.6-scarthgap.sh
NXP i.MX Release Distro SDK installer version 6.6-scarthgap
===========================================================
Enter target directory for SDK (default: /opt/fsl-imx-xwayland/6.6-scarthgap):
You are about to install the SDK to "/opt/fsl-imx-xwayland/6.6-scarthgap". Proceed [Y/n]? Y
Extracting SDK........................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
$ . /opt/fsl-imx-xwayland/6.6-scarthgap/environment-setup-armv8a-poky-linux

 

After this i could'nt find any .wic file. how to get the wic file?
if i am continuing the procedure mentioned in the community post what will be the outcome?

please check the shared image, and walk me through if anything went wrong.

0 Kudos
Reply
45,564 Views
Chavira
NXP TechSupport
NXP TechSupport

HI @Et_MM!

To compile  the image (.wic) you have to compile using the next command:

 

bitbake <image recipe>

 

Example:

bitbake imx-image-full

0 Kudos
Reply
45,485 Views
Et_MM
Contributor III

Hi,

I have done bitbake-imx-image-full and in yocto_sdk/bld-wayland/tmp/deploy/images/imx93evk i see 2 wic file please go through the shared image.

Why the wic image name is imx93evk? i told like we are working with imx93 frdm board? can i use the wic file for imx93-frdm board?

0 Kudos
Reply
45,500 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Et_MM!

 

Apparently you have configured the machine to imx93-evk

Try following the steps that we provide in our github.

 

#Install the repo utility:
$: mkdir ~/bin
$: curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$: chmod a+x ~/bin/repo
$: PATH=${PATH}:~/bin

#Download i.MX Linux Yocto Release:
$: mkdir ${MY_YOCTO} # this directory will be the top directory of the Yocto source code
$: cd ${MY_YOCTO}
$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml
$: repo sync

If errors on repo init, remove the .repo directory and try repo init again.

#Integrate meta-imx-frdm recipes into the Yocto code base:
$: cd ./sources
$: git clone https://github.com/nxp-imx-support/meta-imx-frdm.git
$: cd meta-imx-frdm
$: git checkout imx-frdm-2.0

 

Change to the top directory of the Yocto source code and execute the command below to setup environment for build.

 

#For i.MX93 FRDM
$: MACHINE=imx93frdm DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-setup.sh -b frdm-imx93

 

Run the command below to generate Yocto images:

$: bitbake <image recipe>
 

Some image recipes:

Image Name Description
imx-image-core core image with basic graphics and no multimedia
imx-image-multimedia image with multimedia and graphics
imx-image-full image with multimedia and machine learning and Qt

 

Best Regards!

Chavira

0 Kudos
Reply
45,097 Views
Et_MM
Contributor III

Hi,

Thank you for your reply. i am able to create wic file for imx93frdm board.

0 Kudos
Reply
46,230 Views
Et_MM
Contributor III

Hi,

Do you have any idea about the error seen in the shared image?

I got this error after the system freeze, nearly after two hrs from freeze. please help me with this.

 

0 Kudos
Reply
46,222 Views
Chavira
NXP TechSupport
NXP TechSupport

HI @Et_MM!

 

Apparently your network connection is not stable, I can see the network sign in notification.

 

 

0 Kudos
Reply
46,204 Views
Et_MM
Contributor III

Hi,

Thank you for the reply.

In that case then i will try with a new system, because there is no network issue after that and the freeze issue still persists.

46,247 Views
Et_MM
Contributor III

Hi,

I have tried with the below config, but still freezing.

BB_NUMBER_THREADS = "1"
PARALLEL_MAKE = "-j 1"

Again i tried with 4 thread and 4 core ,at that time the process was running and freeze at some other point, i kept my system as such for 2 hrs suddenly some logs came (please go through the shared image).

If there is no other solutions then i will try it in another system and will update.

 

 

0 Kudos
Reply