i.MX 8 M Plus Current Source and Sink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8 M Plus Current Source and Sink

722件の閲覧回数
Will_Robertson
Contributor III

Hi,

I'm very sorry to ask such a basic question.

Roughly how much current can be sourced or sinked directly by pins configured as output pins on the i.MX 8 M Plus using 3.3 V logic?

I was able to find the different output strengths that could be set in the reference manual but I haven't been able to find how much current can safely be sourced or sinked to these pins.

Will

0 件の賞賛
返信
4 返答(返信)

703件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @Will_Robertson!

Thank you for contacting NXP Support!

 

That information can be consulted in the datasheet.

 

Best Regards!

Chavira

 

0 件の賞賛
返信

701件の閲覧回数
Will_Robertson
Contributor III

Hi @Chavira 

I read the data sheet before asking and couldn't find this information in the data sheet. It may be in the reference document which is 7428 pages long but I haven't been able to read all 7428 pages.

Will

0 件の賞賛
返信

692件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @Will_Robertson!

 

We mention that values but not in a table.

 

We provide a formula to calculate but the typical values for iMX8MP are the next:

 

DSE_X1:  120 Ω
DSE_X2: 60 Ω
DSE_X4:  30 Ω
DSE_X6: 20 Ω

 

With the impedance values you can calculate the maximum current if you are using 3.3v or 1.8v

 

Best Regards!

Chavira

0 件の賞賛
返信

683件の閲覧回数
Will_Robertson
Contributor III

Hi @Chavira 

Thank you very much. The ability to set the output impedance is very valuable and innovative functionality in the i. MX 8M Plus and gives it a significant advantage over other SoCs where an additional chip would be needed to achieve this.

This will significantly ease electronic design and reduce chip count in many systems as well as giving much better fault tolerance leading to better long term robustness and reliability

Will

0 件の賞賛
返信