IMX93-EVK GPIO SET AND GET COMMAND NOT WORKING

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX93-EVK GPIO SET AND GET COMMAND NOT WORKING

1,198 Views
Abisha
Contributor I

I am working on the i.MX93-EVK board. I flashed the imx-image-full-imx93evk.wic file from the LF_v6.6.52-2.2.0_images_IMX93EVK folder. When I try to set GPIO 14 to 1, it only changes the direction of the pin but does not set the pin to high.

Abisha_0-1737527772758.png

Abisha_1-1737527781473.png

 

Tags (1)
0 Kudos
Reply
1 Reply

1,180 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Abisha!

Thank you for contacting NXP Support!

 

The gpiochip that manage the gpio14 (J1001 pin is the gpiochip0

 

Chavira_0-1737563010434.png

 

Chavira_1-1737563044014.png

 

Best Regards!

Chavira

 

 

0 Kudos
Reply