IMX8mp- kernel-module-isp-vvcam_4.2.2.24.0.bb:do_compile, Error.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8mp- kernel-module-isp-vvcam_4.2.2.24.0.bb:do_compile, Error.

4,248件の閲覧回数
MJD
Contributor III

Hello NXP,


lab3@daikokunw-Server:~/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video$ bitbake imx-image-full
Loading cache: 100%  Time: 0:00:00
Loaded 5339 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.4.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mp-lpddr4-evk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.1-mickledore"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:a57506c46d92bf0767060102d2139be06d46f575"
meta-oe
meta-multimedia
meta-python = "HEAD:922f41b39f364e5b6be596b4b51e0fb37ffe1971"
meta-freescale = "HEAD:7327e03c61823268a5a957fe090c4cc5e1735b34"
meta-freescale-3rdparty = "HEAD:bccd93f1ceece608e69799b6fc8f79e8a519f89e"
meta-freescale-distro = "HEAD:7956a0ab407a33c40fdc6eb4fabdcb7dc54fd359"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:c842613830da0a5473513cdbc2dce015b0ca9a5d"
meta-nxp-demo-experience = "HEAD:b8c0a9af3e3ca5400b9aff6436fbb654d3108cb4"
meta-arm
meta-arm-toolchain = "HEAD:c6380674f59489b327c5047d803cc35b68642cd4"
meta-chromium = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6"
meta-clang = "HEAD:af4dcba009ba98250315520f3003fde4ee164cce"
meta-gnome
meta-networking
meta-filesystems = "HEAD:922f41b39f364e5b6be596b4b51e0fb37ffe1971"
meta-qt6 = "HEAD:1406d0a85525a71fe5d7892d7f915404290a78ad"
meta-parsec
meta-tpm = "HEAD:d7db0a3bd1a8639df7570483f003ce00cbe274a2"
meta-virtualization = "HEAD:38e6b3e2fe0219c773f4637a09221ca5d15bf6fc"
meta-daikoku
workspace = "<unknown>:<unknown>"

Initialising tasks: 100% Time: 0:00:03
Sstate summary: Wanted 64 Local 20 Mirrors 0 Missed 44 Current 5284 (31% match, 99% complete)
NOTE: Executing Tasks
ERROR: kernel-module-isp-vvcam-4.2.2.24.0-r0 do_compile: oe_runmake failed
ERROR: kernel-module-isp-vvcam-4.2.2.24.0-r0 do_compile: ExecutionError('/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/temp/run.do_compile.3929678', 1, None, None)
ERROR: Logfile of failure stored in: /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/temp/log.do_compile.3929678
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 32 KERNEL_SRC=/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source KERNEL_PATH=/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source KERNEL_VERSION=6.1.55+g5109ff0b9964 CC=aarch64-poky-linux-gcc -fuse-ld=bfd -fmacro-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam=/usr/src/debug/kernel-module-isp-vvcam/4.2.2.24.0-r0 -fdebug-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam=/usr/src/debug/kernel-module-isp-vvcam/4.2.2.24.0-r0 -fmacro-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2=/usr/src/debug/kernel-module-isp-vvcam/4.2.2.24.0-r0 -fdebug-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2=/usr/src/debug/kernel-module-isp-vvcam/4.2.2.24.0-r0 -fmacro-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2=/usr/src/debug/kernel-module-isp-vvcam/4.2.2.24.0-r0 -fdebug-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2=/usr/src/debug/kernel-module-isp-vvcam/4.2.2.24.0-r0 -fdebug-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/recipe-sysroot= -fmacro-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/recipe-sysroot= -fdebug-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source=/usr/src/kernel -fdebug-prefix-map=/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-build-artifacts=/usr/src/kernel LD=aarch64-poky-linux-ld.bfd AR=aarch64-poky-linux-ar OBJCOPY=aarch64-poky-linux-objcopy O=/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-build-artifacts KBUILD_EXTRA_SYMBOLS=
| make[1]: Entering directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/dwe'
| make -C /home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source ARCH=arm64 M=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/dwe modules
| make[2]: Entering directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source'
| CC [M] /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/dwe/../video/vvbuf.o
| LD [M] /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/dwe/vvcam-dwe.o
| MODPOST /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/dwe/Module.symvers
| LD [M] /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/dwe/vvcam-dwe.ko
| make[2]: Leaving directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source'
| make[1]: Leaving directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/dwe'
| make[1]: Entering directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/isp'
| make -C /home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source ARCH=arm64 M=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/isp modules
| make[2]: Entering directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source'
| CC [M] /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/isp/../video/vvbuf.o
| LD [M] /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/isp/vvcam-isp.o
| MODPOST /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/isp/Module.symvers
| LD [M] /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/isp/vvcam-isp.ko
| make[2]: Leaving directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source'
| make[1]: Leaving directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/isp'
| make[1]: Entering directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video'
| make -C /home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source ARCH=arm64 M=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video modules KBUILD_EXTRA_SYMBOLS=/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video/../dwe/Module.symvers
| make[2]: Entering directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source'
| CC [M] /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video/vvbuf.o
| LD [M] /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video/vvcam-video.o
| MODPOST /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video/Module.symvers
| ERROR: modpost: missing MODULE_LICENSE() in /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video/vvcam-video.o
| make[4]: *** [/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source/scripts/Makefile.modpost:126: /home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video/Module.symvers] Error 1
| make[3]: *** [/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source/Makefile:1966: modpost] Error 2
| make[2]: Leaving directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source'
| make[2]: *** [Makefile:238: __sub-make] Error 2
| make[1]: *** [Makefile:31: all] Error 2
| make[1]: Leaving directory '/home/lab3/YY/imx-yocto-bsp/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-isp-vvcam/4.2.2.24.0-r0/git/vvcam/v4l2/video'
| make: *** [Makefile:8: all] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/lab3/YY/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-kernel/kernel-modules/kernel-module-isp-vvcam_4.2.2.24.0.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 9393 tasks of which 9383 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/lab3/YY/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-kernel/kernel-modules/kernel-module-isp-vvcam_4.2.2.24.0.bb:do_compile
Summary: There were 2 ERROR messages, returning a non-zero exit code.


Guide me to fix this error 

 

0 件の賞賛
返信
1 返信

4,226件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

The error: oe-runmake failed, to check CPU and RAM, like the maximum number of threads bitbake simultaneously executes, and is the size of RAM enough to support the compilation.

13 Speeding Up a Build — The Yocto Project ® 4.3.999 documentation

Notice the one workspace = "<unknown>:<unknown>" in your bblayers.conf, which should not be a proper setting.

Regards

Harvey

 

0 件の賞賛
返信