IMX8mp dsi panel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8mp dsi panel

跳至解决方案
1,846 次查看
joschi2804
Contributor II

Hello,

we want to connect a DSI Panel (IC based on EK79007AD3+EK73217BCGA) to our hardware (based on the Imx8mp module).

We did following changes to our device-tree.

&lcdif1 {
	status = "okay";
};

&mipi_dsi {
	status = "okay";
	port@1 {
		mipi_dsi_out: endpoint {
			remote-endpoint = <&dsi_panel_in>;
		};
	};
	
	panel@0 {
		status = "okay";
		//compatible = "winstar,ek79007ad3";
		compatible = "ronbo,rb070d30";
		reg = <0>;

		port {
			dsi_panel_in: endpoint {
				remote-endpoint = <&mipi_dsi_out>;
			};
		};
	};
};

 

With this setting I get following dmesg output 

dmesg | grep -ri dsi
[    0.836295] imx_sec_dsim_drv 32e60000.mipi_dsi: version number is 0x1060200
[    0.844169] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e60000.mipi_dsi
[    0.912324] imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridge: -517, retry 0
[    1.704951] imx_sec_dsim_drv 32e60000.mipi_dsi: version number is 0x1060200
[    1.712782] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e60000.mipi_dsi
[    1.780977] imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridge: -517, retry 1
[    2.269476] imx_sec_dsim_drv 32e60000.mipi_dsi: version number is 0x1060200
[    2.277300] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e60000.mipi_dsi
[    2.345427] imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridge: -517, retry 2
[    2.474864] imx_sec_dsim_drv 32e60000.mipi_dsi: version number is 0x1060200
[    2.482680] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e60000.mipi_dsi
[    2.550804] imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridge: -517, retry 3
[    2.560036] imx-drm display-subsystem: bound 32e60000.mipi_dsi (ops imx_sec_dsim_ops)

 

It always returns EPROBE_DEFER error code (-517). It seems the panel driver is never loaded correctly. 

I noticed that when I try to load the ronbo kernel module manually, it never calls the probe function. 
I have the same issue that probe function is not called, when I use the "winstar,
ek79007ad3" compatible string (this is panel-simple driver, where I've added a new device).

Is there a reason, why the probe function of the drivers is not called? I thought that if the compatible string matches with the driver, the probe function is called. Or are there further dependencies?

Thanks in advance

 

0 项奖励
回复
1 解答
1,809 次查看
joschi2804
Contributor II

The reason the driver was not calling the probe function was that the driver was integrated as a kernel module instead of being directly compiled into the kernel.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,810 次查看
joschi2804
Contributor II

The reason the driver was not calling the probe function was that the driver was integrated as a kernel module instead of being directly compiled into the kernel.

0 项奖励
回复