IMX8mp - HDMI SSCG issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8mp - HDMI SSCG issue

1,400件の閲覧回数
ZhouLiang1
Contributor III

Hi, experts:

RE radiation (HDMI 148.5MHz). Hope to reduce the EMI by SSCG. But it is not clear how to implement it in I. MX 8 P.I want to ask how to configure it?  Directly operates on the following register(use memtool to modify the register value) that I. MX seems not to execute. The value written to the register is 0x800ff3f0. What kind of operation process is needed to execute the SSCG?

ZhouLiang1_0-1725352652073.png

 

Best regards

Snow

 

0 件の賞賛
返信
2 返答(返信)

1,266件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

I need to ask the experts team I will update with the answer.

Thanks

0 件の賞賛
返信

1,208件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The driver prototype had dependencies across other modules and we may need SW help with the changes.

If you are willing to configure the Modulation Frequency Control and Modulation Rate Control parameters in the function as per the requirements, I can provide you a patch to enable SSCG in the email you posted.

Pls. let me know.

 

0 件の賞賛
返信