IMX8QXP NVMe SSD support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QXP NVMe SSD support

1,260件の閲覧回数
Chethanbg
Contributor III

Dear NXP Team,

We are exploring options to connect an SATA SSD to our custom-designed IMX8QXP board, but we've observed that the processor lacks SATA support. Therefore, we are considering connecting an NVMe-based SSD via the PCIe interface on the M.2 connector instead. Could you confirm if this is feasible? Also, do we have driver support available for this configuration?

0 件の賞賛
返信
1 返信

1,227件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

checked the imx8qxp schematic, which support M.2 KEY E, if you need connect SSD via M.2 connector, you need convert M.2 KEY E to M.2 KEY M to support this, the cable like this

Sintech M.2 (NGFF) NVME SSD to M2 A/E Key WiFi Port with 20cm Cable 

0 件の賞賛
返信