【IMX8QXP,FEC】Does NXP fec driver support MDIO/MDC is clause45

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

【IMX8QXP,FEC】Does NXP fec driver support MDIO/MDC is clause45

2,438件の閲覧回数
jianwei_lan
Contributor III

Dear friend 

my platform is i.MX8QXP, Linux 4.14.98.

Question:1)Does NXP fec driver support clause 45?; 2) Can NXP provide cause 45 patch?

 

-----

BR

0 件の賞賛
返信
3 返答(返信)

2,230件の閲覧回数
MB_Spectrum
Contributor I

Hi has this issue been resolved?

we are working with imx8dxl and SJA1110 and require a clause45 driver for MDIO communication with the ethernet switch. to acces and controll the registers.

 

Br Martijn

0 件の賞賛
返信

2,406件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Sorry, I cannot find the patch. I think we don't patch for this.

0 件の賞賛
返信

2,200件の閲覧回数
nxp82977
NXP Employee
NXP Employee

thats a pitty and also no solution.

 

we did however already patch the HW and added an SPI port to the switch which alowed us to readout the registers.

 

pitty that after 3 weeks still no solution availeble.

pls close the case.

 

0 件の賞賛
返信