IMX8QXP-B0 release details

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QXP-B0 release details

2,876 Views
darsh_dev
Contributor V

Hello Support Team,

Can I use the  latest or > L5.4.24_2_1_0 release for IMX8QXP-B0 revision?

darshak_patel_0-1602680037107.png

In the release note of L5.4.24_2_1_0, mentioned only about the GA for 8QuadXplus C0 only.

Thanks.

0 Kudos
Reply
3 Replies

2,864 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes, you may use it, please make sure that you download the B0 version, I'll leave the link here:
i.MX 8QuadXPlus(B0) MEK

Regards,
Aldo.

0 Kudos
Reply

2,853 Views
darsh_dev
Contributor V

Hi @AldoG ,

Thanks for sharing the L5.4.24-2.1.0_images_MX8QXPMEK. We have custom board and debug LPUART is swaped in our case, so may be this images may not be help to us. Will check it our side.

What about the latest release L5.4.47 ? Because, in yocto machine conf file available for C0 only.

IMX8QXP-C0--L5.4.47.png

Thanks,

 

 

0 Kudos
Reply

2,839 Views
AldoG
NXP TechSupport
NXP TechSupport

Hi,

Please try using the imx8qxpmek machine, you'll find it at meta-freescale/conf/machine.

Regards,
Aldo.

0 Kudos
Reply