IMX8QXP ADC1 Clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QXP ADC1 Clock

1,429 Views
swapnil_ks
Contributor I

Hi I am using IMX8QXP in which i have configured ADC0 , but i have to configure ADC1 and read it ,problem is that there no clock entry for ADC1 ,And if try to use ADC0's clock then it shows following error.

imx8qxp_adc 5a89000.adc: Could not prepare or enable the clock

i have done required changes in device tree, only problem  now is clock for ADC1

so can someone help me, what clock should i use for ADC1

Thanks in Advance  

0 Kudos
Reply
1 Reply

1,368 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I’m afraid that i.MX8QXP family is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply