IMX8QM SMMU Stream IDs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM SMMU Stream IDs

2,751 Views
josemartins90
Contributor II

I'm trying to program the SMMU on an imx8qm. However, I can't find in the documentation the list of the stream peripherals for the various DMA devices. Where can I find this information?

Tags (2)
2 Replies

2,626 Views
igorpadykov
NXP Employee
NXP Employee

Hi josemartins90

all progarmming interfaces are provided with SCU, so one can look

at documentation included in SCFW Porting Kit

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,626 Views
josemartins90
Contributor II

Thank you. I already found out the call that has to be made to setup the SIDs, howver I am not sure if I need to do something else so that the access doesn't bypass the SMMU.

0 Kudos
Reply