IMX8QM SMMU Stream IDs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8QM SMMU Stream IDs

2,750 次查看
josemartins90
Contributor II

I'm trying to program the SMMU on an imx8qm. However, I can't find in the documentation the list of the stream peripherals for the various DMA devices. Where can I find this information?

标记 (2)
2 回复数

2,625 次查看
igorpadykov
NXP Employee
NXP Employee

Hi josemartins90

all progarmming interfaces are provided with SCU, so one can look

at documentation included in SCFW Porting Kit

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,625 次查看
josemartins90
Contributor II

Thank you. I already found out the call that has to be made to setup the SIDs, howver I am not sure if I need to do something else so that the access doesn't bypass the SMMU.

0 项奖励
回复