IMX8QM SMMU Stream IDs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM SMMU Stream IDs

2,810件の閲覧回数
josemartins90
Contributor II

I'm trying to program the SMMU on an imx8qm. However, I can't find in the documentation the list of the stream peripherals for the various DMA devices. Where can I find this information?

ラベル(1)
タグ(2)
2 返答(返信)

2,685件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi josemartins90

all progarmming interfaces are provided with SCU, so one can look

at documentation included in SCFW Porting Kit

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,685件の閲覧回数
josemartins90
Contributor II

Thank you. I already found out the call that has to be made to setup the SIDs, howver I am not sure if I need to do something else so that the access doesn't bypass the SMMU.

0 件の賞賛
返信