IMX8QM OV10635 EVS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM OV10635 EVS

1,314件の閲覧回数
MickyHe
Contributor III

Dear FAE:

we were testing EVS on Android Automotive platform on iMX8QM MEK with MX8XMIPI4CAM2 + MCIMXCAMERA1MP.

We downloaded android auto build image on iMX8QM MEK

--------------------------------------------------------------------

build command :     source build/envsetup.sh
                               lunch mek_8q_car-userdebug

--------------------------------------------------------------------

and 

--------------------------------------------------------------------

build command :     source build/envsetup.sh
                               lunch mek_8q_car2-userdebug

--------------------------------------------------------------------

max9286_mipi 6-006a: ov10635_check_device: OV10635 index=4 was found.

But ov10635_write_reg:write reg error

 

pls check it 

0 件の賞賛
返信
1 返信

1,301件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

Pls refer to the chapter 8.1.1 Interfaces to control the EVS function of enclosed file

0 件の賞賛
返信