IMX8QM: Not able to build kernel with modified defconfig

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM: Not able to build kernel with modified defconfig

ソリューションへジャンプ
5,803件の閲覧回数
vinothkumars
Senior Contributor IV

Hi,

 

IMX8QM-MEK + Android 11 Automotive

 

I am getting following build error with modified kernel defconfig,

 

checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:74] Fetch 'out/target/product/mek_8q/system/etc/vintf/compatibility_matrix.2.xml': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:84] List 'out/target/product/mek_8q/system_ext/etc/vintf/': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:74] Fetch 'out/target/product/mek_8q/system_ext/etc/vintf/manifest.xml': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:84] List 'out/target/product/mek_8q/product/etc/vintf/': No such file or directory
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] files are incompatible: Runtime info and framework compatibility matrix are incompatible: No compatible kernel requirement found (kernel FCM version = 5).
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] For kernel requirements at matrix level 5, Missing config CONFIG_SHADOW_CALL_STACK
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] : Success
INCOMPATIBLE
[ 99% 768/771] Installed file list: out/target/product/mek_8q/installed-files-recovery.txt
[ 99% 769/771] Target vendor fs image: out/target/product/mek_8q/vendor.img
ninja: build stopped: subcommand failed.
18:33:51 ninja failed with: exit status 1

^[[0;31m#### failed to build some targets (03:06 (mm:ss)) ####^[[00m

 

 

 

 

 

 

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
1 解決策
5,786件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you @Bio_TICFSL for the reply.

 

This error occur with modified defconfig. I added my defconfig in automation_defconfig, with that there is no error.

Regards,
Vinothkumar Sekar

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,792件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

It looks like you need to add vintf driver by yourself or if you have driver is incompatible with the kernel version that android 12 have.

 

Regards

0 件の賞賛
返信
5,787件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you @Bio_TICFSL for the reply.

 

This error occur with modified defconfig. I added my defconfig in automation_defconfig, with that there is no error.

Regards,
Vinothkumar Sekar
0 件の賞賛
返信