IMX8QM-MEK Power Management difference between Linux and Android

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8QM-MEK Power Management difference between Linux and Android

跳至解决方案
20,118 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

I got observation when I try to send  suspend-to-ram command ( echo mem > /sys/power/state ) from Android and Linux

Suspend to Ram in Android OS,

      L4.14.98

      # echo mem > /sys/power/state

   

      Application Processor going to suspend and resumed automatically

Suspend to Ram in Linux OS,

      L4.14.78 & L4.14.98

      # echo mem > /sys/power/state

      Application Processor going to suspend and wait for user press power key

Will you please give me the configuration or implementation to achieve the Linux level in Android ?

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
1 解答
19,759 次查看
vinothkumars
Senior Contributor IV

Finally I found wake-up API from power driver and disable it for disabling the auto wakeup.

Regards,

VinothS,

Regards,
Vinothkumar Sekar

在原帖中查看解决方案

0 项奖励
回复
17 回复数
19,760 次查看
vinothkumars
Senior Contributor IV

Finally I found wake-up API from power driver and disable it for disabling the auto wakeup.

Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复
19,759 次查看
smathe25
Contributor III

Hi vinothkumars‌

Could you specify the driver you updated and changes you made to disable auto wake up.

0 项奖励
回复
19,759 次查看
vinothkumars
Senior Contributor IV

Sebimohan Mathew

Find my attachment.

Regards,

Vinoth S,

Regards,
Vinothkumar Sekar
19,759 次查看
smathe25
Contributor III

Thank you so much vinothkumars‌

Have you ever tried GPIO pad wake up with some specific GPIO?

0 项奖励
回复
19,759 次查看
vinothkumars
Senior Contributor IV

Hi Sebimohan Mathew

Please find the document link,

iMX8QM-MEK: SUSPEND AND WAKEUP IN ANDROID 9 AUTOMOTIVE 

Best Regards,

Vinoth S,

Regards,
Vinothkumar Sekar
0 项奖励
回复
19,759 次查看
siva_prabhakara
Contributor III

did u ever get any GPIO wakeup method to work?

0 项奖励
回复
19,758 次查看
smathe25
Contributor III

Follow this: How to add iMX8QXP PAD(GPIO) Wakeup . This worked for me

0 项奖励
回复
19,758 次查看
vinothkumars
Senior Contributor IV

Hi Sebimohan Mathew

I never tried with GPIO. But, some default wake-up already present.

Wake up done by following,

  1. A53 debug UART
  2. Power Key

  • WAKE-UP

    1. BUTTON

         By pressing the power-key SW3 (0.5s)

     2. DEBUG UART

         Enable debug UART wake-up

         # cat ./sys/devices/platform/5a060000.serial/tty/ttyLP0/power/wakeup
         disabled

         # echo enabled  > ./sys/devices/platform/5a060000.serial/tty/ttyLP0/power/wakeup

         TO WAKEUP

                  Press the ENTER Key 2 times

Regards,

Vinoth S,

Regards,
Vinothkumar Sekar
19,751 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinoth

for Android supported power management one can refer to

sect.8.9 Power state configuration attached Android Guide.

from NXP Android documentation on link

Android OS for i.MX Applications Processors | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
19,749 次查看
vinothkumars
Senior Contributor IV

Hi igorpadykov‌

=> power 1 2

I tried Power control from car MCU console

is working, But, Sometimes the system wakes up by itself.

Power control from car MCU consolePower control from car2 AP consoleComment
suspendpower 1 2echo "1 2" > /sys/devices/ platform/vehicle-dummy/ power_reqThe system disconnects from BT, waits for all tasks to be done, and then enter suspend mode. Press the power-on key to wake up the system. BT is connected again. Sometimes the system wakes up by itself.

Is there any possible to disable system wake up ?

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复
19,749 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinoth

one can look at power management differencies between android and linux

Linux Kernel and Android Suspend/Resume -blog archive 

Best regards
igor

0 项奖励
回复
19,749 次查看
vinothkumars
Senior Contributor IV

Hi igorpadykov‌

I validate the Linux L4.14.98 in imx8qm Mek board. There is no auto wake-up.

I compared the Linux pm driver source  with Android 9 automotive (L4.14.98) look like both are same.

Why android and Linux behaving differently when I write the power sate "echo mem > /sys/power/state " ?

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 项奖励
回复
19,749 次查看
igorpadykov
NXP Employee
NXP Employee

Hi VinothS

>Why android and Linux behaving differently when I write the power sate "echo mem > /sys/power/state " ?

because power management is different in linux and android as described below

Linux Kernel and Android Suspend/Resume -blog archive 

Best regards
igor

0 项奖励
回复
19,749 次查看
vinothkumars
Senior Contributor IV

Thank you Igor for your quick reply,

Is it possible to configure Linux power management in Android ?

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复
19,749 次查看
igorpadykov
NXP Employee
NXP Employee

Hi VinothS

this is general android question, suggest to post it on android forums:

Learn about our Developer community programs  |  Google Developers 

Best regards
igor

0 项奖励
回复
19,749 次查看
vinothkumars
Senior Contributor IV

Thank you Igor for the reply.

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复
19,749 次查看
vinothkumars
Senior Contributor IV

Hi Igore,

Thank you for the quick reply. I checked the document and thank you for the document.

I needs to send power 1 2  (=> power 1 2) from M4 console to suspend Application Processor , Am I right ?

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复