IMX8QM Board resetting while flashing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM Board resetting while flashing

2,608件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

I got reset issue while flashing. I don't know what is the issue. Will you please give some points

 

resetting ...
Board: iMX8QM MEK
Boot: USB
DRAM:
SCSI: Net: Fastboot: Normal

 

PS L:\25-03-T2> .\uuu.exe -b emmc .\u-boot-imx8qm-mek-uuu.imx
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.107-0-g9201dde

Success 0 Failure 0


PS L:\25-03-T2> ================100%=================] SDPS: boot -f .\u-boot-imx8qm-mek-uuu.imx

 

While flashing board hanged here.

 

 

 

 

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,587件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

seems this issue is related to

https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8QM-Custom-Board/m-p/1259...

 

Best regards
igor

0 件の賞賛
返信

2,557件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you @igorpadykov  for the reply.

I able to do DDR stress in one of the custom board.

I done the following for DDR initialization in IMX8QM board,

  1. Copy the .cfg content to scfw board directory
  2. Build and copy the scfw binary to uboot firmware
  3. Build bootloader.

 

Please find the complete log. I got the u-boot panic,

Board: iMX8QM MEK .........................START
Boot: USB
announce_dram_init DRAM:
show_dram_config
++ RAM Configuration .......

DRAM:
imx8_iomux_setup_multiple_pads ..............
imx8_iomux_setup_pad ..................
imx8_iomux_setup_pad ..................
imx8_iomux_setup_pad ..................
imx8_iomux_setup_multiple_pads ..............
imx8_iomux_setup_pad ..................
imx8_iomux_setup_pad ..................
SCSI: Net: Fastboot: Normal................END

do_sync ..........
panic -------Resetting CPU ...

panic_finish ..............
++++++++++++++++++++++++ resetting ...

 

 

Will you please give me some ideas why u-boot panic is happening ?

 

 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信

2,490件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you @igorpadykov for the reply.

 

This is the USB C issue. I disable in config after that it's flashing.

 

 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信

2,520件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

just for test one can try to build without OPTee as described in sect.5.6.10 OP-TEE enablement

i.MX Yocto Project User’s Guide​

 

Best regards
igor

0 件の賞賛
返信