IMX8MQ6 BSDL/ID Code mismatch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MQ6 BSDL/ID Code mismatch

ソリューションへジャンプ
2,086件の閲覧回数
ians1
Contributor I

Hello I hope someone can help!

I have a IMX8MQ6CVAHZAB populated twice on my pcba. (TDI = W5, TDO = U5).

When sniffing the device with jtaglive it reads the 'freescale' ID code as 00001000100011100010000000011101

This matches the user manual description of the SJC ID Code

However the BSDL file (IMX8M) lists the ID Code as 00011100111110000000010101010011

JTAG Mod is high, and only one core is detected.

I am also confident the other pins are as per the compliance section.

Can anyone advise if there is a different BSDL file I should be using?

Thanks Ian

0 件の賞賛
返信
1 解決策
2,079件の閲覧回数
Yuri
NXP Employee
NXP Employee

@ians1 
Hello,

  Please check if Your configuration satisfies COMPLIANCE_PATTERNS
in the BSDL file.

attribute COMPLIANCE_PATTERNS of IMX8M: entity is
"(BOOT_MODE0, BOOT_MODE1, GPIO1_IO00, GPIO1_IO01, GPIO1_IO02, " &
"GPIO1_IO03, TEST_MODE) (0000011)";

 https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX8M_BSDL

 Also:

https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Entering-Boundary-Scan-mode/m-p/915500

Regards,
Yuri.

元の投稿で解決策を見る

1 返信
2,080件の閲覧回数
Yuri
NXP Employee
NXP Employee

@ians1 
Hello,

  Please check if Your configuration satisfies COMPLIANCE_PATTERNS
in the BSDL file.

attribute COMPLIANCE_PATTERNS of IMX8M: entity is
"(BOOT_MODE0, BOOT_MODE1, GPIO1_IO00, GPIO1_IO01, GPIO1_IO02, " &
"GPIO1_IO03, TEST_MODE) (0000011)";

 https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX8M_BSDL

 Also:

https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Entering-Boundary-Scan-mode/m-p/915500

Regards,
Yuri.