IMX8MQ6 BSDL/ID Code mismatch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ6 BSDL/ID Code mismatch

Jump to solution
2,161 Views
ians1
Contributor I

Hello I hope someone can help!

I have a IMX8MQ6CVAHZAB populated twice on my pcba. (TDI = W5, TDO = U5).

When sniffing the device with jtaglive it reads the 'freescale' ID code as 00001000100011100010000000011101

This matches the user manual description of the SJC ID Code

However the BSDL file (IMX8M) lists the ID Code as 00011100111110000000010101010011

JTAG Mod is high, and only one core is detected.

I am also confident the other pins are as per the compliance section.

Can anyone advise if there is a different BSDL file I should be using?

Thanks Ian

0 Kudos
Reply
1 Solution
2,154 Views
Yuri
NXP Employee
NXP Employee

@ians1 
Hello,

  Please check if Your configuration satisfies COMPLIANCE_PATTERNS
in the BSDL file.

attribute COMPLIANCE_PATTERNS of IMX8M: entity is
"(BOOT_MODE0, BOOT_MODE1, GPIO1_IO00, GPIO1_IO01, GPIO1_IO02, " &
"GPIO1_IO03, TEST_MODE) (0000011)";

 https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX8M_BSDL

 Also:

https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Entering-Boundary-Scan-mode/m-p/915500

Regards,
Yuri.

View solution in original post

1 Reply
2,155 Views
Yuri
NXP Employee
NXP Employee

@ians1 
Hello,

  Please check if Your configuration satisfies COMPLIANCE_PATTERNS
in the BSDL file.

attribute COMPLIANCE_PATTERNS of IMX8M: entity is
"(BOOT_MODE0, BOOT_MODE1, GPIO1_IO00, GPIO1_IO01, GPIO1_IO02, " &
"GPIO1_IO03, TEST_MODE) (0000011)";

 https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX8M_BSDL

 Also:

https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Entering-Boundary-Scan-mode/m-p/915500

Regards,
Yuri.