Hi NXP Team,
In one of the hardware designs we are planning to establish a communication link between two IMX8MQ processors. For that we are planning to use the PCIe as the communication medium. The reason we are trying to establish a connection using PCIe is to save the PHY space in the circuit.
On the hardware front, we are planning to establish communication using as per the below diagram.
Hi Harshit
yes this design is feasible, also one can look at below link
(as pcie module is similar to i.MX6)
i.MX6Q PCIe EP/RC Validation System
For software use linux pcie driver described on
i.MX Software and Development Tools | NXP
or baremetal sdk (1.1.0_iMX6_Platform_SDK.zip) on link SMP Enable in IMX6
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Thank you for your reply and confirmation of the hardware connections.
We are planning to use the Linux reference here. From the Linux release notes manual I verified that the EP and RC mode support is there in i.MX8MQ processor.
Regards.
Hi Harshit
1, yes in this case internal PCIe clock can be used.
For other questions please create new threads.
Best regards
igor