Hi,
I am trying to connect IMX8MQ with intel FPGA thru PCIE+DMA, IMX8 as RP and FPGA as EP.
I've succeed to read/write a 4KB size data from/to RP thru FPGA's DMA, but it failed when changed to the larger size, e.g 16KB.
When I captured signals on DMA, it was founded that only 1 cycle of read operation happened, then DMA hang up with BUSY status, and bytes_left is 16,384.
Anyone who knows why ? Sincerely hope for your help!
Hi, igor
Thanks for reply.
I am now using 4.19.35, IMX8MQ EVK, it is almost the newest.
One point to be confirmed, I found below description in processor reference manual:
Does it mean the DMA operation must be splited into 4K pieces for a large size data ?
Hi Chenguang
sorry 4.19.35 is not newest, please check latest on
Embedded Linux for i.MX Applications Processors | NXP
Best regards
igor
Hi Chenguang
what bsp used in the case, could you try latest
Embedded Linux for i.MX Applications Processors | NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------