IMX8MQ Uboot cannot read or write the MIPI DSI register
09-30-2020
02:21 AM
2,058 次查看
Our products use IMX8MQ, we hope to achieve MIPI DSI output display in the UBOOT phase. It was found that IMX8MQ could not read or write directly to the registers of the MIPI DSI, which would cause the direct chip reset and then enter the wireless loop.
In the uboot-imx/board/freescale/imx8mq_evk/imx8mq_evk.c,We tested reads and writes in the board_init function
4 回复数
09-30-2020
03:48 AM
2,053 次查看
igorpadykov
NXP Employee
Hi Dio_HUI
for example one can look at uboot mipi-dsi driver
Best regards
igor
10-08-2020
08:20 PM
2,036 次查看
hi: igorpadykov
int mipi_dsi_northwest_setup(u32 base_addr, u32 sim_addr){
dsi_info->sim_base = sim_addr;
}
I donot know which register is match the sim_addr on i.MX8MQ platform, can you point it out?
05-19-2021
02:30 AM
1,857 次查看
my_name_lyl
Contributor I
IMX8MQ 的 mipi-dsi 的寄存器地址 is 0x30a00000 ,可以参考linux内核的设备树文件(dtb)