IMX8MQ UART2(SER2) problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MQ UART2(SER2) problem

2,434件の閲覧回数
prathap_ponnuch
Contributor I

Hi all,

I am trying UART3(SER2 TX and RX) communication.

Following setting are done:

/* ser2 */&uart3 {         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_uart3>;         assigned-clocks = <&clk IMX8MQ_CLK_UART3>;         assigned-clock-parents = <&clk IMX8MQ_CLK_25M>;         uart-has-rtscts;         status = "okay"; };
             /* ser 2 */                pinctrl_uart3: uart3grp {                         fsl,pins = <                                /* SER2_RX */                                MX8MQ_IOMUXC_ECSPI1_SCLK_UART3_DCE_RX           0xe                                /* SER2_TX */                                MX8MQ_IOMUXC_ECSPI1_MOSI_UART3_DCE_TX           0xe                                /* SER2_CTS_N */                                MX8MQ_IOMUXC_ECSPI1_MISO_UART3_DCE_CTS_B        0xe                                /* SER2_RTS_N */                                MX8MQ_IOMUXC_ECSPI1_SS0_UART3_DCE_RTS_B         0xe                        >;                 }; 
After this, in console side we given the following command: note:ttymxc2(tx and rx pin, rts)connected to other host at 115200 baudrate.
root@sm2s-imx8m-qc:~# stty -echo raw speed 115200 < /dev/ttymxc2115200 root@sm2s-imx8m-qc:~# echo "testing" > /dev/ttymxc2              root@sm2s-imx8m-qc:~#    After this commands there is no output in host system?
May i know what is the problem and how to check this uart?
Thanks in advance.

Regards,
prathap

					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,374件の閲覧回数
prathap_ponnuch
Contributor I

Hi Igor,

Thanks for replay.

we are using the following path to modify:

linux-imx/4.14.98-r0/git/arch/arm64/boot/dts/msc$ vi msc-sm2s-imx8m-qc-001.dts

Regards,

prathap

0 件の賞賛
返信

2,374件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prathap

 

if  this is third party software may be suggested to post issue to tech support

of vendor of that software.

 

Best regards
igor

0 件の賞賛
返信

2,374件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prathap

what bsp used in the case, for uart3 dts example one can look at

imx8mq-evk.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

test with uart unit test and Demo Image:

mxc_uart_test\test - imx-test - i.MX Driver Test Application Software 

Demo Image i.MX 8M Quad EVK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信