IMX8MQ 8G LPDDR4 change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ 8G LPDDR4 change

Jump to solution
3,017 Views
coindu
Contributor IV

Hi community:

        I have a qustion about use 8G LPDDR4 instead of 3G lpddr4 on IM8MQ.

       Firstly download the laster ddr tools with mscale_ddr_tool _v3.20 and MX8M_LPDDR4_RPA_v29.xlsx.

       Then open the DDR datasheet, I can see the below infomation

coindu_0-1626232571266.png

 

       row aaddress is [16:0]

       so I modify the RPA file 

       

coindu_1-1626232622555.png

        copy DDR strees test file to xxxx.ds and run the mscale DDR tool. the result is raw 16, something wrong?   Does the tool can support to 8G?

        

coindu_2-1626232728002.png

    and how the modify the uboot code about it. 

Labels (1)
0 Kudos
Reply
1 Solution
3,010 Views
igorpadykov
NXP Employee
NXP Employee

Hi Coin

 

unfortunately lpddr4 devices with 17-row addresses are not supported by i.MX8MQ.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
3,011 Views
igorpadykov
NXP Employee
NXP Employee

Hi Coin

 

unfortunately lpddr4 devices with 17-row addresses are not supported by i.MX8MQ.

 

Best regards
igor

0 Kudos
Reply
3,005 Views
coindu
Contributor IV

        Does it means that 8G DDR cannot be support?According to the chip manual, it supports 8GLPDDR configuration.Do you have any successful experience with 8G LPDDR?

Tags (1)
0 Kudos
Reply