IMX8MP debug port change to uart4 on Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MP debug port change to uart4 on Android

ソリューションへジャンプ
865件の閲覧回数
FoxYang
Contributor I

Hi,

In imx8mp on customer board.

I have already change debug port from uart2 to uart4 on yocto(Linux 6.1.1_1.0.1 BSP).

And type cmd is OK.

 

The same modify on Android (Android 13.0.0_2.0.0 (L6.1.22_2.0.0 BSP)),

after booting finish(hdmi show android launcher),debug console can show message

but can't type anything.

 

I have compare yocto and android modify.

There are 2 file I can't find in Android BSP.

\sources\meta-freescale\conf\machine\include\imx-base.inc

\sources\meta-freescale\conf\machine\include\imx8mp-evk.inc

 

How to fix it?

Thanks.

 

0 件の賞賛
返信
1 解決策
813件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

You are looking for Yocto specific files, that are not available on Android.
For Android you'll need to patch Linux/Uboot/ATF the same way you did for the Linux system you built using Yocto.

Best regards/Saludos,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
814件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

You are looking for Yocto specific files, that are not available on Android.
For Android you'll need to patch Linux/Uboot/ATF the same way you did for the Linux system you built using Yocto.

Best regards/Saludos,
Aldo.

0 件の賞賛
返信