IMX8MP check NPU usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MP check NPU usage

5,829 次查看
Eric97
Contributor II

Hello,

I'm using IMX8MP with the system Yocto Linux. I'd like to check NPU usage, such as the "%CPU" from the command "top". I have noticed the description like "Arm® Cortex®-A53 with an integrated NPU". Does it mean that the NPU is integrated into the CPU, so it can't be checked alone? If so, does the CPU usage also include the usage of the integrated NPU?

Thanks,

0 项奖励
回复
4 回复数

4,664 次查看
Hitesh_em
Contributor I

Did anyone found any solution, to see NPU utilization % realtime

0 项奖励
回复

5,823 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Jichen,

It can be checked but when you use one of the machine learning tools please check it:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MP-NPU-debug-and-fine-tune-applicat...

 

Regards

0 项奖励
回复

5,818 次查看
Eric97
Contributor II

Thanks a lot. 

Using machine learning tools like NPU PROFILER, we can obtain the processing time of each operator on the NPU. What I need is to get the NPU usage in real time like the percentage of NPU that is being used by the process. 

For example, using command "top", we can get the %CPU. Can we get similar information for NPU? 

Jichen_vs_0-1658398045835.png

Or does the CPU information we get include NPU? Because I see the NPU is an integrated NPU in Arm® Cortex®-A53 CPU.

3,331 次查看
ooper901
Contributor II
Any updates on that?
0 项奖励
回复