IMX8MP Uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP Uboot

Jump to solution
5,774 Views
AsadNawaZ_93
Contributor II

My bootloader stucks here.

U-Boot SPL 2022.04-lf_v2022.04+g16e8414193 (Oct 08 2022 - 13:33:43 +0000)
No pca9450@25
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from BOOTROM
Boot Stage: Primary boot
image offset 0x8000, pagesize 0x200, ivt offset 0x0
Can't support legacy image
SPL: failed to boot from all boot devices

ERROR ### Please RESET the board

###############################################

Tags (1)
0 Kudos
Reply
1 Solution
5,698 Views
AsadNawaZ_93
Contributor II

Thanks for your reply. I have found the solution already. It was an issue of wrong UART address for ATF "ATF_BOOT_UART_BASE". After setting it correctly as per the UART address on carrier board (Renasas SMARC), I got it working.

View solution in original post

0 Kudos
Reply
4 Replies
5,699 Views
AsadNawaZ_93
Contributor II

Thanks for your reply. I have found the solution already. It was an issue of wrong UART address for ATF "ATF_BOOT_UART_BASE". After setting it correctly as per the UART address on carrier board (Renasas SMARC), I got it working.

0 Kudos
Reply
5,753 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
5,745 Views
AsadNawaZ_93
Contributor II

Thanks for your reply. Please find the detailed explanation in one of my other ticket. 

https://community.nxp.com/t5/i-MX-Processors/U-boot-Bootloader-not-loading-for-ADLINK-LEC-IMX8MP/td-...

 

0 Kudos
Reply
5,740 Views
joanxie
NXP TechSupport
NXP TechSupport

I've replied to you in that tread, what media do you use? SD card?

0 Kudos
Reply