IMX8MP-EVK CPU Module and Base board Altium design files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MP-EVK CPU Module and Base board Altium design files

跳至解决方案
6,239 次查看
massimoincerti
NXP Employee
NXP Employee

Hi, 

 

Customer SKF: is asking for Altium format design files for 8Mplus-EVK Base Board and CPU Module.

As alternative the .ALG files of the two boards which might in case be imported into Altium Tool.

thanks and best regards

Massimo Incerti

 

 

0 项奖励
回复
1 解答
6,225 次查看
Yuri
NXP Employee
NXP Employee

@massimoincerti 
Hello,

  I've sent You the files  via e-mail.

Regards,
Yuri.

 

 

在原帖中查看解决方案

12 回复数
4,133 次查看
ukayacik
Contributor I

@Yuri can you pls send the library files of EVK?

0 项奖励
回复
4,649 次查看
SMBAES
Contributor I

Hi Support Team, I am also looking for the ASCII version of these design files. ".alg". Can you please provide them?

 

Best Regards,

 

Stuart Mill

0 项奖励
回复
5,977 次查看
zmlopez
Contributor III

Hi,

May I also get the .ALG files of 8MPLUSLPD4-CPU and 8MPLUS-BB ?

Regards and thanks in advance

 

0 项奖励
回复
5,971 次查看
Yuri
NXP Employee
NXP Employee

@zmlopez 
Hello,

   We do not provide design files for Altium.

Customers can try the following approach:

https://www.altium.com/documentation/knowledge-base/altium-designer/how-to-import-allegro-binary-fil...

 

Regards,
Yuri.

0 项奖励
回复
6,226 次查看
Yuri
NXP Employee
NXP Employee

@massimoincerti 
Hello,

  I've sent You the files  via e-mail.

Regards,
Yuri.

 

 

2,016 次查看
Tolgabzkn
Contributor I

Dear Yuri,


Could you please send the Altium files for the 8MPLUSLPD4-CPU and 8MPLUS-BB designs?

Thanks,

Tolga Bozkan

0 项奖励
回复
5,378 次查看
mtoibero
Contributor I

Dear Yuri,

I´m also looking for tha altium files for the bb46370 and for the pvk46881 boards.

I have the .alg files converted from the .brd original files, but i´m missing the footprints.

Can you help me?

I need to design a custom base board with only a few peripherals with strong space constraints (thinking on 100K boards and the lack of the complete altium project is delaying the project.

Thanks in advance.

marcos.-

0 项奖励
回复
5,878 次查看
sergeidanielian
Contributor I

Hi, Yuri.

Can you please send a reference on where we can load schematic/reference files - we are planning to start working on SOM based on i.MX8M.

The board we have and ideally for which we need design files is 8MPLUSPLD4-EVK

 

Thanks in advance.

Sergei Danielian

0 项奖励
回复
6,040 次查看
diegoperez
Contributor II

Hi Yuri,

 

I am designing a new platform based on imx8mp, it would be useful for me to have the .alg files (or Altium files) of the CPU and BaseBorad EVK.

 

Thanks in advance.

Diego.

0 项奖励
回复
6,029 次查看
Yuri
NXP Employee
NXP Employee

@diegoperez 
Hello,

  I'ce sent You some comments.

Regards,
Yuri.

0 项奖励
回复
6,217 次查看
massimoincerti
NXP Employee
NXP Employee

Thanks Yuri.