[IMX8MP][DWE] Dewarp Engine clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[IMX8MP][DWE] Dewarp Engine clarification

2,426 Views
ms_emsys
Contributor I

From IMX8MPRM, Rev. 1, 06/2021:

The Dewarp Engine cannot be used as a standalone module.

1. Is this a hardware limitation (shared clock control etc)?

2. Is this a software limitation because the userspace stack (isp-imx) does not support this usecase?

2. Would it be possitble to use the isi_0 or isp_0 to do the format conversion from RAW8 GRAYSCALE into a format compatible with the dwe?

 

0 Kudos
Reply
2 Replies

2,218 Views
malik_cisse
Senior Contributor I

From iMX8MP_CAMERA_DISPLAY_GUIDE.pdf Figure 17 (see below). it appears that dewarp output is a separate output from ISP and one should be able to access it in parallel to accessing ISP output on /dev/video0 device node.
Is this understanding correct? If yes, how can I access Dewarp output? I have activated Dewarp but I only see /dev/video0 device node.

dewarp.jpg

 Any usage example of Dewarp will be welcome.
THX

0 Kudos
Reply

2,404 Views
joanxie
NXP TechSupport
NXP TechSupport

I have mailed to you and give you detailed answer, pls check your mailbox

 

0 Kudos
Reply