IMX8MP CSI meta data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP CSI meta data

818 Views
jjiimmyy
Contributor II

Hi,

Our sensor has to send 1920 x (2 rows front metadata + 1536 + 4 rows end metadata).

From previous post, I am aware IMX8MP cannot handle metadata.

Sensor can configure metadata data type, which I can make it the same as the image type.

1. From reading the ISP porting guide,  it seems embedded data can be "crop" out. But there is a restriction on the input sensor size; it needs height to be 8 align. Is this true?

2. Should I set image size in the ISP XML file and DEWARP to include metadata or just the active image resolution ?

1920 x 1542 (including metadata)

1920 x 1536 (active image)

 

 

Screenshot from 2024-08-07 18-05-36.pngScreenshot from 2024-08-07 18-05-36.pngScreenshot from 2024-08-07 18-07-30.pngScreenshot from 2024-08-07 18-07-30.png

 

 

 

 

 

 

 

0 Kudos
Reply
1 Reply

761 Views
jimmychan
NXP TechSupport
NXP TechSupport

FYI . Please read the section 7 of this document.

i.MX 8M Series MIPI Capture System

0 Kudos
Reply