IMX8MP Booting from ECSPI2 is inconsistent

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MP Booting from ECSPI2 is inconsistent

185件の閲覧回数
YorkerHazan
Contributor I

Greetings, 
We have encountered an issue with attempting to boot from ECSPI2.
We changed the boot flags in the fuses to force boot from ECSPI2 (ECSPI2 is connected to a NOR Flash which is programmed with a valid boot image).

Booting is inconsistent, most of the times the booting will fail but occasionally it will succeeded.  

To verify that this is an issue with the SOC, we switched to using the imx8mp-evb.

after performing the same fuse selection for the SOC on the evb we checked the spi transactions using an oscilloscope, which gave us the following findings:
1) The SCK dutycycle is 75% (where is should be 50% to my understanding) 
2) The SCK is 1.7v (where it should be 3.3v, should be identicle to MOSI which is 3.3v)

(These measurements are correct for the EVB and for our proprietary hardware)

I would greatly appreciate any help regarding this issue as it is a big issue for us! 

ラベル(1)
0 件の賞賛
返信
1 返信

169件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @YorkerHazan 

Booting is inconsistent, most of the times the booting will fail but occasionally it will succeeded. 

>>>please check your hardware connection. It seems your HW connection error.

B.R

0 件の賞賛
返信