IMX8MP - AD1939 audio codec capture issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP - AD1939 audio codec capture issue

Jump to solution
2,146 Views
Airbus_A320
Contributor II

Hi,

I'm having some trouble with an AD1939 codec. I need my application to work in TDM mode (8 playback streams on a single lane and 4 capture streams on a single lane) and the CPU to be the clock master. I managed to get the codec recognized by the kernel and it playbacks OK. I'm having a hard time getting the capture streams configured.

Here is a snippet of my device tree:

/ {
	sound-ad193x {
		compatible = "simple-audio-card";
		simple-audio-card,name = "ad193x-audio";
		simple-audio-card,format = "dsp_a";
		simple-audio-card,frame-master = <&cpudai>;
		simple-audio-card,bitclock-master = <&cpudai>;
		simple-audio-card,mclk-fs = <256>;

		cpudai: simple-audio-card,cpu {
			sound-dai = <&sai2>;
			dai-tdm-slot-num = <8>;
			dai-tdm-slot-width = <32>;
		};

		codecdai:simple-audio-card,codec {
			sound-dai = <&codec_audio_analog>;
		};
	};
};

&ecspi2 {
	codec_audio_analog: ad1939_spi@0 {
		compatible = "ad1939";
		reg = <0>;
		spi-max-frequency = <1000000>;
		#sound-dai-cells = <0>;
		status = "okay";
	};
};

&sai2 {
	#sound-dai-cells = <0>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_sai2>;
	assigned-clocks = <&clk IMX8MP_CLK_SAI2>;
	assigned-clock-parents = <&clk IMX8MP_AUDIO_PLL1_OUT>;
	assigned-clock-rates = <12288000>;
	clocks = <&audio_blk_ctrl IMX8MP_CLK_AUDIO_BLK_CTRL_SAI2_IPG>, <&clk IMX8MP_CLK_DUMMY>,
		 <&audio_blk_ctrl IMX8MP_CLK_AUDIO_BLK_CTRL_SAI2_MCLK1>, <&clk IMX8MP_CLK_DUMMY>,
		 <&clk IMX8MP_CLK_DUMMY>;
	clock-names = "bus", "mclk0", "mclk1", "mclk2", "mclk3";
	fsl,dataline = <0 0x1 0x1>;
	fsl,sai-mclk-direction-output;
	status = "okay";
};

&iomuxc {
	pinctrl_sai2: sai2grp {
		fsl,pins = <
            MX8MP_IOMUXC_SAI2_TXC__AUDIOMIX_SAI2_TX_BCLK 	0x000000D6
            MX8MP_IOMUXC_SAI2_TXD0__AUDIOMIX_SAI2_TX_DATA00	0x00000196
            MX8MP_IOMUXC_SAI2_TXFS__AUDIOMIX_SAI2_TX_SYNC	0x000000D6
			MX8MP_IOMUXC_SAI2_RXD0__AUDIOMIX_SAI2_RX_DATA00 0x000000D6
		>;
	};
};

 

The configuration sent by the codec driver over the SPI bus looks fine to me. Here is a screenshot of the signals I get:

20221024-0003.png

When I try to record I get just noise. Reproducing the wave file through my logic analyzer looks like the whole 8-slot frame gets "compressed" into 4 frames (muting first channel one and then channel two while recording I see during playback that the most significant bit of channel one got zeroed first then the least significant ones). Another symptom is that if I lunch arecord with a duration flag it records for exactly twice the time!

~# time arecord -fs16 -r48000 -c4 /dev/null --duration 2
Recording WAVE '/dev/null' : Signed 16 bit Little Endian, Rate 48000 Hz, Channels 4

real	0m4.136s
user	0m0.056s
sys	0m0.024s

My theory is the bit clock inside the receiver got somehow halved...
Peeking at the sai registers during the recording I see MSEL in RCR2 is 00, I was expecting it to be 01 as in TCR2.

If I configure the codec to be the clock master all works as expected.

 

Can anybody please help me?
Thanks

0 Kudos
Reply
1 Solution
2,120 Views
Airbus_A320
Contributor II

Answering myself in case somebody needs a hint on a similar issue.

The problem was I had clocked the SAI peripheral at the same rate my bit clock is. I have 8 32-bit slots at 48 kHz, so my bit clock is 12.288 MHz and in my device tree I had assigned-clock-rates = <12288000>

Running out of ideas I tried to reduce the slot count to 4 (bit clock 6.144 MHz) and all went fine. So I tried to revert to 8 slots and increase assigned-clock-rates to twice the bit clock. Now I can playback and capture w/o any issue.

 

View solution in original post

0 Kudos
Reply
1 Reply
2,121 Views
Airbus_A320
Contributor II

Answering myself in case somebody needs a hint on a similar issue.

The problem was I had clocked the SAI peripheral at the same rate my bit clock is. I have 8 32-bit slots at 48 kHz, so my bit clock is 12.288 MHz and in my device tree I had assigned-clock-rates = <12288000>

Running out of ideas I tried to reduce the slot count to 4 (bit clock 6.144 MHz) and all went fine. So I tried to revert to 8 slots and increase assigned-clock-rates to twice the bit clock. Now I can playback and capture w/o any issue.

 

0 Kudos
Reply