Hello
We are currently trying to bring up our ethernet phy on our custom board using a digi imx8mn nano som and an Analog Devices ADIN1200 using the MDIO and RMII interface. The imx8mn shall provide the 50MHz clk_ref for the rmii interface to the phy and its internal MAC as described in the IMX reference manual Table 11-42 and ADIN datasheet page 12 table 14. When powering up the board the phy is not found with the following message:
root@ccimx8mn-cc-a:~# dmesg | grep eth
[ 2.098277] mdio_bus 30be0000.ethernet-1: MDIO device at address 0 is missing.
[ 2.106146] fec 30be0000.ethernet eth0: registered PHC device 0
[ 5.796575] fec 30be0000.ethernet eth0: Unable to connect to phy
However we can see a clock signal on the mdc line and some activity on the mdio line. We can not observe a clock signal on the ETH_REF_CLK line. If we give the phy id manually in the device tree with `compatible = "ethernet-phy-id0282.bc20", "ethernet-phy-ieee802.3-c22";` an eth0 shows up but is not operational. Using mii-diag tool it reports no valid mii device.
The device tree and the relevant parts of the schematic are shown below.
Schematic
```` device tree
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec1_gpio>,
<&pinctrl_fec1>;
phy-mode = "rmii";
phy-handle = <ðphy0>;
/* Set the proper voltage regulator. */
// assigned-clock-rates = <0>, <100000000>, <125000000>, <50000000>;
phy-reset-gpios = <&gpio4 27 GPIO_ACTIVE_LOW>;
phy-reset-duration = <1>;
fsl,magic-packet;
status = "okay";
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@0 {
/*
* cc-a board is equipted with the ADIN12000 phy
* see https://www.digi.com/resources/documentation/digidocs/embedded/dey/4.0/cc8mnano/bsp- ethernet_r_8m
* and https://wiki.analog.com/resources/tools-software/linux-drivers/net-phy/adin
*/
// compatible = "adi,adin";
// compatible = "ethernet-phy-id0282.bc20", "ethernet-phy-ieee802.3-c22";
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
adi,fifo-depth-bits = <8>;
status = "okay";
interrupt-parent = <&gpio3>;
interrupts = <25 IRQ_TYPE_EDGE_FALLING>;
};
};
};
&iomuxc {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_hog>;
pinctrl_fec1: fec1grp {
fsl,pins = <
MX8MN_IOMUXC_ENET_MDC_ENET1_MDC 0x3
MX8MN_IOMUXC_ENET_MDIO_ENET1_MDIO 0x23
MX8MN_IOMUXC_ENET_TD0_ENET1_RGMII_TD0 0x1f
MX8MN_IOMUXC_ENET_TD1_ENET1_RGMII_TD1 0x1f
MX8MN_IOMUXC_ENET_RD0_ENET1_RGMII_RD0 0x91
MX8MN_IOMUXC_ENET_RD1_ENET1_RGMII_RD1 0x91
MX8MN_IOMUXC_ENET_TX_CTL_ENET1_RGMII_TX_CTL 0x1f
MX8MN_IOMUXC_ENET_RX_CTL_ENET1_RGMII_RX_CTL 0x91
MX8MN_IOMUXC_ENET_RXC_ENET1_RX_ER 0x91
MX8MN_IOMUXC_ENET_TD2_ENET1_TX_CLK 0x4000001f
>;
};
pinctrl_fec1_gpio: fec1gpiogrp {
fsl,pins = <
/* PHY reset */
MX8MN_IOMUXC_SAI2_MCLK_GPIO4_IO27 0x16
/* PHY interrupt */
MX8MN_IOMUXC_SAI5_MCLK_GPIO3_IO25 0x41
>;
};
};
````