Hi:
I recently ported the USB to serial driver for the XR21V1414 driver to the 8mm platform. I’m using BSP 5.4.3, but I keep encountering the following error when reading data, which is causing the read and write functions to malfunction.[ 1195.875954] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 0.474366] usbcore: registered new interface driver usbfs
[ 0.479443] usbcore: registered new interface driver hub
[ 0.484797] usbcore: registered new device driver usb
[ 1.327154] usbcore: registered new interface driver usb-storage
[ 1.333257] usbcore: registered new interface driver option
[ 1.338858] usbserial: USB Serial support registered for GSM modem (1-port)
[ 1.688715] usbcore: registered new interface driver usbhid
[ 1.694297] usbhid: USB HID core driver
[ 2.098379] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator
[ 2.107256] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator
[ 3.708212] imx_usb 32e40000.usb: 32e40000.usb supply vbus not found, using dummy regulator
[ 3.762945] imx_usb 32e50000.usb: 32e50000.usb supply vbus not found, using dummy regulator
[ 4.093960] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[ 4.150020] usb 2-1: new high-speed USB device number 2 using ci_hdrc
[ 4.557678] usb 1-1.3: new full-speed USB device number 3 using ci_hdrc
[ 4.785680] usb 1-1.4: new full-speed USB device number 4 using ci_hdrc
[ 4.869657] usb 1-1.4: device no response, device descriptor read/64, error -32
[ 5.061961] usb 1-1.4: device no response, device descriptor read/64, error -32
[ 5.253742] usb 1-1.4: new full-speed USB device number 5 using ci_hdrc
[ 5.337712] usb 1-1.4: device no response, device descriptor read/64, error -32
[ 5.529688] usb 1-1.4: device no response, device descriptor read/64, error -32
[ 5.645938] usb 1-1-port4: attempt power cycle
[ 6.253712] usb 1-1.4: new full-speed USB device number 6 using ci_hdrc
[ 6.673765] usb 1-1.4: device not accepting address 6, error -32
[ 6.762024] usb 1-1.4: new full-speed USB device number 7 using ci_hdrc
[ 7.185710] usb 1-1.4: device not accepting address 7, error -32
[ 7.193077] usb 1-1-port4: unable to enumerate USB device
[ 25.571373] xr_usb_serial_common: loading out-of-tree module taints kernel.
[ 25.580993] cdc_xr_usb_serial 1-1.3:1.0: USB_device_id idVendor:04e2, idProduct 1414
[ 25.581007] cdc_xr_usb_serial 1-1.3:1.0: This device cannot do calls on its own. It is not a modem.
[ 25.590139] cdc_xr_usb_serial 1-1.3:1.0: The data interface has switched endpoints
[ 25.590144] cdc_xr_usb_serial 1-1.3:1.0: interfaces are valid
[ 25.590157] cdc_xr_usb_serial 1-1.3:1.0: epwrite->bEndpointAddress =1
[ 25.590332] cdc_xr_usb_serial 1-1.3:1.0: ttyXR_USB_SERIAL0: USB XR_USB_SERIAL device
[ 25.600607] cdc_xr_usb_serial 1-1.3:1.2: USB_device_id idVendor:04e2, idProduct 1414
[ 25.600617] cdc_xr_usb_serial 1-1.3:1.2: This device cannot do calls on its own. It is not a modem.
[ 25.609777] cdc_xr_usb_serial 1-1.3:1.2: The data interface has switched endpoints
[ 25.609782] cdc_xr_usb_serial 1-1.3:1.2: interfaces are valid
[ 25.609792] cdc_xr_usb_serial 1-1.3:1.2: epwrite->bEndpointAddress =2
[ 25.609958] cdc_xr_usb_serial 1-1.3:1.2: ttyXR_USB_SERIAL1: USB XR_USB_SERIAL device
[ 25.620722] cdc_xr_usb_serial 1-1.3:1.4: USB_device_id idVendor:04e2, idProduct 1414
[ 25.620733] cdc_xr_usb_serial 1-1.3:1.4: This device cannot do calls on its own. It is not a modem.
[ 25.629940] cdc_xr_usb_serial 1-1.3:1.4: The data interface has switched endpoints
[ 25.629948] cdc_xr_usb_serial 1-1.3:1.4: interfaces are valid
[ 25.629959] cdc_xr_usb_serial 1-1.3:1.4: epwrite->bEndpointAddress =3
[ 25.630129] cdc_xr_usb_serial 1-1.3:1.4: ttyXR_USB_SERIAL2: USB XR_USB_SERIAL device
[ 25.640077] cdc_xr_usb_serial 1-1.3:1.6: USB_device_id idVendor:04e2, idProduct 1414
[ 25.640087] cdc_xr_usb_serial 1-1.3:1.6: This device cannot do calls on its own. It is not a modem.
[ 25.649235] cdc_xr_usb_serial 1-1.3:1.6: The data interface has switched endpoints
[ 25.649246] cdc_xr_usb_serial 1-1.3:1.6: interfaces are valid
[ 25.649255] cdc_xr_usb_serial 1-1.3:1.6: epwrite->bEndpointAddress =4
[ 25.649423] cdc_xr_usb_serial 1-1.3:1.6: ttyXR_USB_SERIAL3: USB XR_USB_SERIAL device
[ 25.662333] usbcore: registered new interface driver cdc_xr_usb_serial
[ 25.668930] xr_usb_serial_common: Exar/MxL USB UART (serial port) driver version 1D
[ 1184.043100] tty ttyXRUSB2: xr_usb_serial_tty_install
[ 1184.044199] tty ttyXRUSB2: xr_usb_serial_tty_open
[ 1184.044209] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_port_activate
[ 1184.045153] xusb set rs485
[ 1184.046554] cdc_xr_usb_serial 1-1.3:1.4: 0xa1
[ 1184.047905] cdc_xr_usb_serial 1-1.3:1.4: 0x20
[ 1184.047912] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.047919] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.047925] cdc_xr_usb_serial 1-1.3:1.4: 0x04
[ 1184.047931] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.047937] cdc_xr_usb_serial 1-1.3:1.4: 0x02
[ 1184.047943] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.047949] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.047955] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.047966] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_ctrl_irq - input control lines: dcd- dsr- break- ring- framing- parity- overrun-
[ 1184.048263] xusb enabled rs485
[ 1184.050279] cdc_xr_usb_serial 1-1.3:1.4: 0xa1
[ 1184.051337] cdc_xr_usb_serial 1-1.3:1.4: 0x20
[ 1184.051340] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.051344] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.051348] cdc_xr_usb_serial 1-1.3:1.4: 0x04
[ 1184.051351] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.051354] cdc_xr_usb_serial 1-1.3:1.4: 0x02
[ 1184.051357] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.051363] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.051366] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.051375] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_ctrl_irq - input control lines: dcd- dsr- break- ring- framing- parity- overrun-
[ 1184.051527] xusb set logical level to 0
[ 1184.052141] cdc_xr_usb_serial 1-1.3:1.4: 0xa1
[ 1184.056023] cdc_xr_usb_serial 1-1.3:1.4: 0x20
[ 1184.056027] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.056030] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.056034] cdc_xr_usb_serial 1-1.3:1.4: 0x04
[ 1184.056037] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.056040] cdc_xr_usb_serial 1-1.3:1.4: 0x02
[ 1184.056043] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.056046] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.056049] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.056056] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_ctrl_irq - input control lines: dcd- dsr- break- ring- framing- parity- overrun-
[ 1184.057269] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_tty_set_termios - set line: 115200 0 0 8
[ 1184.060266] cdc_xr_usb_serial 1-1.3:1.4: 0xa1
[ 1184.060278] cdc_xr_usb_serial 1-1.3:1.4: 0x20
[ 1184.060281] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.060284] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.060288] cdc_xr_usb_serial 1-1.3:1.4: 0x04
[ 1184.060291] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.060294] cdc_xr_usb_serial 1-1.3:1.4: 0x02
[ 1184.060297] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.060300] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.060303] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.060309] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_ctrl_irq - input control lines: dcd- dsr- break- ring- framing- parity- overrun-
[ 1184.062272] cdc_xr_usb_serial 1-1.3:1.4: 0xa1
[ 1184.062280] cdc_xr_usb_serial 1-1.3:1.4: 0x20
[ 1184.062283] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.062286] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.062289] cdc_xr_usb_serial 1-1.3:1.4: 0x04
[ 1184.062292] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.062295] cdc_xr_usb_serial 1-1.3:1.4: 0x02
[ 1184.062301] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.062304] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.062307] cdc_xr_usb_serial 1-1.3:1.4: 0x00
[ 1184.062313] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_ctrl_irq - input control lines: dcd- dsr- break- ring- framing- parity- overrun-
[ 1195.866433] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_tty_close
[ 1195.866453] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_port_shutdown
[ 1195.869457] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_ctrl_irq - urb shutting down with status: -2
[ 1195.872573] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.872655] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.872691] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.872718] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.872744] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.872781] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.875877] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.875954] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.875985] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.876011] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.876042] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.879128] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.879198] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.879223] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.879244] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.881682] cdc_xr_usb_serial 1-1.3:1.5: xr_usb_serial_read_bulk_callback - non-zero urb status: -2
[ 1195.881783] cdc_xr_usb_serial 1-1.3:1.4: xr_usb_serial_tty_cleanup
However, the same driver works fine on BSP 4.14, so it seems that there may be a bug in the USB driver code for BSP 5.4. Could you help me fix the issue?
已解决! 转到解答。
Hello,
Beware of this driver, it works okay when reading data with those errors, but my MX8MM died and rebooted randomly.
That's why I won't risk it and have unloaded the module, if not reading data.
You better try on 6.1v BSP:
Regards