IMX8MM stuck in android boot logo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM stuck in android boot logo

1,622 Views
bansidaranaccor
Contributor I

Hi,

We are working on iMX8M Mini EVK board. Flashed android 10 on imx8m mini evk board. While booting it hangs on android boot logo. And getting some error related to 'vendor.thermal-hal-2-0' service.

Tried android-10.0.0_2.6.0 Demo Image on imx8mm evk board same issue exist.

Below are the logs related to vendor.thermal error. Also attached complete log for reference.

[ 38.814525] init: Received control message 'start' for 'bootanim' from pid: 326 (/system/bin/surfaceflinger)
[ 38.825047] init: starting service 'bootanim'...
[ 40.703635] init: starting service 'vendor.thermal-hal-2-0'...
[ 40.821973] init: Untracked pid 489 exited with status 0
[ 40.827651] init: Service 'vendor.thermal-hal-2-0' (pid 486) received signal 6
[ 40.834966] init: Sending signal 9 to service 'vendor.thermal-hal-2-0' (pid 486) process group...
[ 40.844182] libprocessgroup: Successfully killed process cgroup uid 1000 pid 486 in 0ms
[ 40.852839] init: Untracked pid 491 exited with status 0
[ 41.965549] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 45.714579] init: starting service 'vendor.thermal-hal-2-0'...
[ 45.842000] init: Untracked pid 546 exited with status 0
[ 45.847782] init: Service 'vendor.thermal-hal-2-0' (pid 543) received signal 6
[ 45.855134] init: Sending signal 9 to service 'vendor.thermal-hal-2-0' (pid 543) process group...
[ 45.864332] libprocessgroup: Successfully killed process cgroup uid 1000 pid 543 in 0ms
[ 45.873075] init: Untracked pid 548 exited with status 0
[ 50.727553] init: starting service 'vendor.thermal-hal-2-0'...

Kindly provide solution for above issue.

Regards,

Bansidaran

0 Kudos
Reply
0 Replies