IMX8MM eMMC1 boot SPL error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM eMMC1 boot SPL error

1,163件の閲覧回数
tanyagroysberg
Contributor II

Hi,

We have a custom board based on the IMX8M Mini LPDDR4 EVK, but the boot procedure is configured to use eMMC1. The eMMC is accessible via USB boot (fastboot) and can be flashed correctly. However, when attempting to boot from it, the process gets stuck in the SPL state, with the device not receiving the CMD response.

The ROM successfully loads the SPL from the eMMC.

The pinout is configured in the spl.c board file, while U-Boot uses the device tree file.

The boot fails in the boot_from_devices function in common/spl/spl.cit recieves no responce from mmc_send_op_cond_iter function.

The configuration patches both for u-boot and spl are also attached, is there a configuration error in SPL definitions?

Thanks,

Tanya

0 件の賞賛
返信
1 返信

1,121件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @tanyagroysberg 

Please modofy the spl.c file at location board/freescale/imx8mm_evk/spl.c file and try again. Not common/spl/spl.c.

B.R

0 件の賞賛
返信