IMX8MM USB Compliance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM USB Compliance

1,947件の閲覧回数
jonas_blick
Contributor I

Hi,

I seen serveral post on the tools/document needed for USB2.0 (HS eye) test for the IMX8Mini,

I also need this documents/files in order to do some compliance testing.

Thank you.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

1,291件の閲覧回数
hms1234
Contributor I

Hi

Can i get access to https://community.nxp.com/docs/DOC-329745 

/henrik

0 件の賞賛
返信

1,816件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jonas

document was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,816件の閲覧回数
penny_lin
Contributor III

Hi igor:

  Could you share the document to me , I also need this documents/files in order to do some compliance testing.

Thank your help.

Penny Lin

0 件の賞賛
返信

1,816件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Penny 

suggest to create service request https://community.nxp.com/docs/DOC-329745 

Best regards
igor

0 件の賞賛
返信

1,657件の閲覧回数
christophapel
Contributor I

Hi Igor,

I would also need access to the necessary patches to run USB test mode.

access to https://community.nxp.com/docs/DOC-329745 is denied.

thanks and regards, Christoph

0 件の賞賛
返信

1,652件の閲覧回数
christophapel
Contributor I

to be precise, I have "I.MX6/7/8 series USB Certification Guide" available but cannot locate "How to do USB Compliance Test for 4.x kernel_v2.5" which is supposed to describe the necessary BSP patches.

0 件の賞賛
返信