IMX8MM: RPMsg between A core and M4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM: RPMsg between A core and M4

2,013件の閲覧回数
roger_chang
Contributor I

I am using a IMX8MM in my project and running android 9 on this. In the project, we plan to have some GPIO function working on M4, and there will be some communications between A core and M4.

I have download the RPMsg-lite sample for reference, but I still have no idea what's the mechanism for avoiding resources overlap on both A core and M4. Is the multicore manager responsible for the resource allocation and monitoring between multiple core? If it is, where can I find the sample code? (I only found RPMsg-lite under the multicore example folder)

ラベル(1)
0 件の賞賛
返信
1 返信

1,902件の閲覧回数
b36401
NXP Employee
NXP Employee

For the tests you can play with RPMsg test program included into unit-test of our Linux.
Please refer to chapter 2.8.5 "Running i.MX RPMsg Test Programs" of 2.8.5 of i.MX Linux Reference Manual included to this bundle:
https://www.nxp.com/docs/en/supporting-information/fsl-yocto-L4.9.123_2.3.0_mx8mm.zip

0 件の賞賛
返信