IMX8M reset implementation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M reset implementation

ソリューションへジャンプ
2,597件の閲覧回数
vadimaleynikov
Contributor III

The i.MX 8MDQLQ Hardware Developer’s Guide in Table 7 recommends that the reset button should be connected to the PMIC enable pin. In this case, the iMX8M reset is impelmented by swithching off all the IMX8M power (except probably SNVS). 

What is the reason of a such drastic reset way?

Whether a less radical method of resetting the IMX8M exist (which doesn't require switching power off)?

Best regards,
Vadim Aleynikov

0 件の賞賛
返信
1 解決策
2,181件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

such reset solution is similar one used on i.MX6Q Sabre SD board designs,

please check p.21 spf-27392 "PWRON" signal.

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

or ENGR00338067 mentioned in AN5161 p.24

https://www.nxp.com/docs/en/application-note/AN5161.pdf 

Swithching off all the IMX power is fool proof universal reset solution, probably one can use other solutions

but this require detailed schematic analysis for implications when some components remain

in non-reset state. There is no usiversal solution and each case should be separately considered.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,182件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

such reset solution is similar one used on i.MX6Q Sabre SD board designs,

please check p.21 spf-27392 "PWRON" signal.

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

or ENGR00338067 mentioned in AN5161 p.24

https://www.nxp.com/docs/en/application-note/AN5161.pdf 

Swithching off all the IMX power is fool proof universal reset solution, probably one can use other solutions

but this require detailed schematic analysis for implications when some components remain

in non-reset state. There is no usiversal solution and each case should be separately considered.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,181件の閲覧回数
vadimaleynikov
Contributor III

Thank you, Igor.

Vadim

0 件の賞賛
返信