IMX8M processor Image sensor supported and RGB LCD interface with i.MX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M processor Image sensor supported and RGB LCD interface with i.MX8M

2,122 Views
karan_chauhan
Contributor II

Hi joanxie‌ and karinavalencia‌,

I have following question:

1. We have Parallel RGB666/888 LCD and want to connect it with the i.MX8MQ processor. Can anyone suggest me the suitable solutions? Any bridge or converter which NXP has been suggested for this type of application which could work straight forward.

2. Does the i.MX8MQ processor supports  the IMX290 (2MP @30fps) sony image sensor ?

3. What other types of image sensor supported in the i.MX8MQ processor?

Best Regards,

Karan Chauhan

0 Kudos
Reply
2 Replies

1,976 Views
joanxie
NXP TechSupport
NXP TechSupport

1) i.MX8M doesn't have parallel interface, supports mipi lcd

2)yes, can support it, mipi csi can support up to Support 5M pixel at 15 fps

3)can support  for all CSI-2 data types

0 Kudos
Reply

1,976 Views
karan_chauhan
Contributor II

Hi joanxie‌,

Thank you for response!

Could please answer it my below questions:

1. We have Parallel RGB666/888 LCD and want to connect it with the i.MX8MQ processor. Can anyone suggest me the suitable solutions? Any bridge or converter which NXP has been suggested for this type of application which could work straight forward.

Regards,

Karan Chauhan

0 Kudos
Reply