IMX8M | modify Yocto device tree

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8M | modify Yocto device tree

5,961 次查看
shai_b
Senior Contributor II

Dear team,

My customer would like to find the location of the imx8m device tree source (DTS) in order to modify a few parameters.

1. Could you please advise where the source code of these files are located?

2. What is the best way to compile only the device tree and add the complied file (DTB) into u-boot?

Wating for your kind feedback, many thanks.

KR,

Shai

 

0 项奖励
回复
2 回复数

5,904 次查看
karl1688
Contributor II

Use "bitbake linux-imx -c devshell" open a new terminal, the path for example

<local build folder>/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source

 

Change dts file in <local build folder>/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.32+gitAUTOINC+fa6c316859-r0/git/arch/arm64/boot/dts/freescale/

 

Then do "make dtbs" in new terminal, the new dtb general in <local build folder>/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.32+gitAUTOINC+fa6c316859-r0/build/arch/arm64/boot/dts/freescale/

0 项奖励
回复

5,946 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 项奖励
回复