IMX8M mini LPDDR4 ERROR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M mini LPDDR4 ERROR

2,151件の閲覧回数
jianfeichang
Contributor IV

imx8m mini LPDDR4 2G samsung,it is error

0x40000000  and 0x80000000 are the same.Write data at address 0x40000000 3,0x80000000 also.

0x50000000  and 0x90000000 are the same.

0x60000000  and 0xa0000000 are the same.

NOW,why?

pastedImage_1.jpg

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,013件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jianfei

reason may be hardware errors (some lines are shorted), Also one

can try to change drive strengths and ODT settings, check if that helps.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,013件の閲覧回数
jianfeichang
Contributor IV

hi

I have a different situation in the uboot, the address seems to operate independently。

read 0x4000 0000 and 0x8000000 ,The data is the same.

but write 0x80000000 aaaa,and read 0x40000 0000, The data is different.

QQ图片20191101192924.png

0 件の賞賛
返信

2,013件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

also this may be soldering issue, so one can try to resolder chip.

Best regards
igor

0 件の賞賛
返信