IMX8M mini LPDDR4 ERROR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8M mini LPDDR4 ERROR

2,143 次查看
jianfeichang
Contributor IV

imx8m mini LPDDR4 2G samsung,it is error

0x40000000  and 0x80000000 are the same.Write data at address 0x40000000 3,0x80000000 also.

0x50000000  and 0x90000000 are the same.

0x60000000  and 0xa0000000 are the same.

NOW,why?

pastedImage_1.jpg

标记 (1)
0 项奖励
回复
3 回复数

2,005 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jianfei

reason may be hardware errors (some lines are shorted), Also one

can try to change drive strengths and ODT settings, check if that helps.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,005 次查看
jianfeichang
Contributor IV

hi

I have a different situation in the uboot, the address seems to operate independently。

read 0x4000 0000 and 0x8000000 ,The data is the same.

but write 0x80000000 aaaa,and read 0x40000 0000, The data is different.

QQ图片20191101192924.png

0 项奖励
回复

2,005 次查看
igorpadykov
NXP Employee
NXP Employee

also this may be soldering issue, so one can try to resolder chip.

Best regards
igor

0 项奖励
回复