IMX8M Plus LPDDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Plus LPDDR4

Jump to solution
1,975 Views
Anderswikstrom
Contributor I

Hi,

Is it possible to only connect one channel (A or B) for IMX8M Plus, to interface a 16-bit LPDDR4 memory?

Br

Anders

0 Kudos
Reply
1 Solution
1,967 Views
Yuri
NXP Employee
NXP Employee

@Anderswikstrom 
Hello,

   generally, since LPDDR4 device consists of two identical channels operating independently, it is possible to configure single channel x16 mode.

   Below are discussions regarding the issue.

https://community.nxp.com/t5/i-MX-Processors/Single-channel-LPDDR4/m-p/818564

https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387065

 

 

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
1,968 Views
Yuri
NXP Employee
NXP Employee

@Anderswikstrom 
Hello,

   generally, since LPDDR4 device consists of two identical channels operating independently, it is possible to configure single channel x16 mode.

   Below are discussions regarding the issue.

https://community.nxp.com/t5/i-MX-Processors/Single-channel-LPDDR4/m-p/818564

https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387065

 

 

Regards,
Yuri.

0 Kudos
Reply