IMX8M PLUS LPDDR4 2G compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M PLUS LPDDR4 2G compatibility

3,954 Views
TMpieye
Contributor I

We try to implement an ISSI IS43LQ32512A-046BLI 2GB RAM. After Calibration the RAM fails during the  memcpy SSN armv8_x32 test with 2000MHz configured.

If I configure the RAM to 1500MHz it pass all the tests.

Has anybody implement this LPDDR4 RAM? Is it in general compatible with IMX8M PLUS?

0 Kudos
Reply
12 Replies

3,173 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @TMpieye 

Did you run the stress test with our DDR Config Tool? From your log file, it seems not from the Config Tool output. Also use out latest tool version v25.12.

B.R

0 Kudos
Reply

3,103 Views
TMpieye
Contributor I

Hello @pengyong_zhang ,

I run the tes in the config tool and and its passed. So it seems to be a tool problem with the MSCALER tool. Many thanks for your great support!

0 Kudos
Reply

3,166 Views
TMpieye
Contributor I

hHi @pengyong_zhang 

for stresstest we use the Mscale DDR Tool 3.31. I will do it with the other config tool

0 Kudos
Reply

3,423 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @TMpieye 

It's strange. Please share your DDR Config Tool v25.12 fail log

B.R

0 Kudos
Reply

3,193 Views
TMpieye
Contributor I

Hello @pengyong_zhang ,

 

here is the log of the stresstest. We have the same Problem wirth an 4GB ISSI IS43LQ32K01S2A-046BLI. 

0 Kudos
Reply

3,600 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @TMpieye 

Please use below setting run the DDR test.

pengyong_zhang_0-1769394027487.png

B.R

0 Kudos
Reply

3,442 Views
TMpieye
Contributor I
Thanks for your Config Exaple. Its the same I already tryed with this RAM and still get the error.
0 Kudos
Reply

3,755 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @TMpieye

Please use the below link download our DDR Config Tool and run the ddr test wIth configure 2GB dram. 

https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-developm...

B.R

0 Kudos
Reply

3,741 Views
TMpieye
Contributor I

Hello @pengyong_zhang ,

Same result with the config Tool V 13.1. Maybe our configuration is wrong for the IS43LQ32512A-046BLI? Can you provide the correct configuration (*.ds file)? Our hardware desing is a 1:1 copy of the eval board regarding the LPDDR4 interface. 

Kind Regards

Tobias

0 Kudos
Reply

3,904 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @TMpieye 

Are you using DDR config tool run the Calibration? If yes,. please share your configuration page and fail log file.

B.R

0 Kudos
Reply

3,813 Views
TMpieye
Contributor I

Thanks for your support.

In Attachments i send you the configuration .xls and the test log.

0 Kudos
Reply

3,805 Views
TMpieye
Contributor I
On the used board we have sucsesslully runing 3GB (MT53E768M32D2ZW-046 WTC) and 4GB (MT53E1G32D2FW-046 AAT:B)
Micron LPDDR4 on 2000MHz.
0 Kudos
Reply