IMX8M Nano: Test GPU without MIPI-DSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Nano: Test GPU without MIPI-DSI

1,348 Views
joshua_jhan
Contributor III

Hi All,

I want to test GPU function in INX8M Nano customer board without any display device.

I try to use the /opt/imx-gpu-sdk/ and /opt/viv_samples/ tool to test GPU , but most of the tools cannot be executed and return the following log.

vdk_create_display(955): wl_display_connect failed

 

Thanks,

0 Kudos
Reply
1 Reply

1,338 Views
igorpadykov
NXP Employee
NXP Employee

Hi Joshua

 

seems lcd is always used, one can try to modify rm67191 driver, comment functions where driver

expects answer from lcd

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mn-evk-r...

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/panel/panel-raydium-rm6719...

 

Best regards
igor

0 Kudos
Reply