IMX8M Mini secure boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Mini secure boot

1,085 Views
filipvuko
Contributor I

Hi everyone,


I'm trying to wrap my head around building yocto image with secure boot for IMX 8M mini. So far researching google has lead me to a lot of 404 links and other dead ends. Can you please provide me with some guidance? 

 

Thank you

0 Kudos
Reply
3 Replies

1,059 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

You can refer to <10.9 Automated image signing for secure boot in i.MX application processors> from the Linux User Guide: i.MX Linux User's Guide (nxp.com.cn)

 

Regards

Harvey

0 Kudos
Reply

1,045 Views
filipvuko
Contributor I

What kind of security features are there on imx 8m mini and plus? 

For example:
HABv4?
CAAM? 
etc...

0 Kudos
Reply

1,024 Views
Harvey021
NXP TechSupport
NXP TechSupport

Yes, there are security features, HABV4, CAAM...etc. You can refer to the corresponding SRM for different chip for more details.

Download Security Reference Manual for i.MX 8M Mini Applications Processor (nxp.com)

 

Regards

Harvey

0 Kudos
Reply