IMX8M Mini input transition time on GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Mini input transition time on GPIO

1,331 Views
Sylvain_B
Contributor II

Hello,

 

I haven't found any specification for the transition time of GPIO inputs when CMOS input is selected with registers (Hysteresis Enable field bit disable).

Where can I find it?

Regards.

0 Kudos
Reply
2 Replies

1,304 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Sylvain_B 

I hope you are doing well.

 

Unfortunately we have not documented your exact requirement but you can take a look to the AN5078 (Influence of Pin Setting on System Function and Performance).

 

Best regards,

Salas.

0 Kudos
Reply

1,290 Views
Sylvain_B
Contributor II

Hello,

Thanks your for your reply.

On the oscillograms, the horizontal scale  ((??ns/div) is not visible. and this is not mentioned in the explanations. It's a pity, because if I'd been able to read it, I'd have been able to evaluate the input transition time. 

Regards

0 Kudos
Reply