IMX8M JTAG Circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M JTAG Circuit

4,632 Views
leandroschmitz
Contributor I

Hello, 

I having problems to debug M4 software on IMX8M, I follow the guide on Using JLink Debugger for M4 software on IMX8M but J-LINK Server Can't find any processor on JTAG.

I think witch the problem may be in my JTAG circuit, mainly the o use of a pull-down on JTAG_TCK.

Can you help me reviewing my JTAG circuit.

Thanks 

Regards 

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

4,129 Views
pantarun_92
Contributor I

JTAG_TCK has internal 27K Pull up, why is a10K pull down required?

0 Kudos
Reply

4,295 Views
igorpadykov
NXP Employee
NXP Employee

Hi Leandro

i.MX8M EVK uses the same connection so seems there is no problem using it.

Schematics
Design Files for the i.MX 8M Evaluation Kit (EVK)(REV 0)

i.MX 8M Evaluation Kit | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,295 Views
sinanakman
Senior Contributor III

Hi Leandro

How is you JTAG_MOD connected ? Is it properly pulled down ?

Regards

Sinan Akman

0 Kudos
Reply